Part Number: XTR111-2EVM
Other Parts Discussed in Thread: XTR111
I have just bought a XTR111 EVM board. However, I have encountered several problems with the board.
I have followed the procedures for the basic EVM configuration. But, I still cannot obtained a current output of 4 to 20 mA with the voltage input of 0 to 5 V.
The supplied voltage is +24V as per mentioned in the user guide. I