Hi,
For a customer I am looking for a high speed opamp that can handle including DC up to AC with a GBP up to 4GHz and a voltage noise density spec of <2nVrtHz.
Drift is less important since the environment is temp stable and can be compensated.
Another requirement is that the ampifier has to be placed in a non inverting topology, gain +2.25 with the input signal at the + input.
The + input impedance has to be high compared to the source impedance that can vary between 40 and 100Ohms. Gain should have no influence on the source impedance.
The input signal can go between zero and +0.4V, so the input has to be able to cope with signals to ground (single supply is preferred)
Ideally the output has to be differential to drive a shielded cable.
Do we have such a solution available?