Part Number: TLV342
Hi,
I see the X2QFN package is really small. With +3.3V and -2.2V power supply, if the output voltage is -2V DC, how much current can it sink and source? I need a 10/10mA under 75C operation temperature.
If the power rails are ±2.5V, what the sink/source current would be?
You could also recommend other small package for dual/quad channels. Smaller than TLV342 is welcome.
Thanks.