This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1100: Protect the AMC1100 when the shunt is open

Part Number: AMC1100

Hi,

In my application I need to measurement the load bidirectional current with a isolated power supply. The load is a DC with max 60Vdc/200A (max ±250mv ).

I wanted to use the AMC1100 Fully-Differential Isolation Amplifier in a High-Side measurement configuration (with floating 5V power supply, VCC1) and I want protect the AMC1100 when the shunt is open.

Can I use the circuit here without measurement accuracy problems ? 

Thanks