Part Number: LM231
Other Parts Discussed in Thread: LM331,
Team,
My customer has the following question:
We are looking for insight on a parameter on the LM221, LM331 datasheet.
There is a parameter in the electrical characteristics that lists the conversion accuracy for the LM221 as 0.95 to 1.05 kHz/V
We're trying to piece together the overall accuracy of the device to see if we can avoid test selection of a motor speed loop. If we were running the device between 1Hz and 700Hz, would the design be affected by a gain error of +/-5%?
Regards,
Aaron