Other Parts Discussed in Thread: DSD1791
Hi,
I need to design a sinewave oscillator with following spec.
Frequency: 90Hz to 1KHz
Amplitude: upto 12V variable using potentionmeter
Frequecny Accuracy: <0.1%
THD: <0.05%
Frequency stability: 15ppm/degC
Amplitude Stability:100uV/degC
I was thinking of designing as follows.
Use a microcontroller which is working with a highly stable crystal oscillator. and generate square wave from uC.
send squarewaves to MAX7400 and 8th order filter to generate sivewave. Use an amplifier at output to vary the amplitude from 0-10V.
Can anybody tell me whether any good idea other than the above is there, which will take care almost all the requirements mentioned above.
Thanks.