Part Number: XTR116
Other Parts Discussed in Thread: XTR115, XTR117
Hi!
I know it's odd, but will this circuit work as intended?
I = Ii*(1 + R1/R2)?
The external R2 (shown) will be 25.5 ohm. R1 (shown) will be between 1k and 10k ohm (tbd).
The internal R1 + R2 = 2.5k will be across the op-amp input terminals - is this a problem?
The internal Rlim of course will not be in effect (I may put an external current limiting resistor in series with the emitter).
Thanks!
Also, for some reason the forum changes to Precision Data Converters when XTR115 or XTR116 are selected.