Part Number: OPA188
Other Parts Discussed in Thread: INA149, OPA2188, OPA2192
Hi,
I have to accurately measure a differential voltage of +-80V or +-8V or +-2V upon +-400V common mode voltage. The OPA188 offers really good noise and offset parameters, ideal to measure DC, but with a bias current of 1.5nV this will induce a high error voltage at the resistors I need. Any idea how to solve this problem?
Input is differential, output is differential (so I Need 2 OPA188, no problem), Input Impedanz should be >400M Output volatge should be +-4V F.S. for all three ranges. Supply is +-15V.
With best regards
Gerhard