Other Parts Discussed in Thread: LMH5401
hi all:
My hardware is as follow:
1)The ADS5400 is internal reference;
2)LMH5401 is powered by single power supply: VS+ is 5V and VS- is GND;
3)The output of LMH5401 is followed by a low-pass filter as disribed in Figure 37 of ADS5400's datesheet;
4)without input the output of ADS5400 is all 12'h800;
5)Now when I input a sin signal by a signal generator, the output of ADS5400 is as follow:
The simulation result is as follow:
Why?
=============================================================================
Now, I add a resister as follow:
The output of ADS5400 is ok for input signal power below -10dBm, But without input signal, the output of ADS5400 is so big.(signed Decimal almost 980)
Thanks!