We have large electrolytic capacitors (~1mF) connected directly to the inputs of LMH6629 WSON8. Power supply is +5V and capacitors get charged to 2.5V during normal operation. When device is powered down to 0 volts, input capacitors will be discharging through the inputs of LMH6629, effectively powering up the LMH6629 and the rest of the board for some time.
It looks like LMH6629 does have protective diodes to discharge such input capacitors: in our case they are discharged by the LMH6629 inputs to about 0.6 volts within 0.1 second and 30mA peak current.
Q1: What would be the maximum safe charge that internal protective diodes can discharge? Or: for how long we can run 30mA through the inputs?
Q2: Is there any particular external diode or other solution that you would recommend to protect LMH6629 inputs from large input currents? (we were thinking about BAT68 diode).