Part Number: OPA1632
Other Parts Discussed in Thread: PCM1804,
Hello,
I would like to use the OPA1632 to drive a high Performance ADC PCM1804. Referring to the datasheet of the OPA1632 page 13, the signal Inputs 8 and 1 of the OPA1632 are not on the DC-Level Vcom, right?
If I want to get them there, one possibility would be to use a big capacitor for AC coupling in series with R1, R2. Is it alternatively possible to go with a symmetrical Input signal to R1, R2, which is allready on DC-potential VCOM? This would mean no DC current is flowing out of OPA1632 and through the resistors R1,R2.
Some comments on that would help a lot.
Thanks in advance