Part Number: THS4304
Other Parts Discussed in Thread: OPA693, , THS4302
Dear experts,
Customer is looking for high speed amp to replace OPA693(Gain =2) which is used for 130MHz clock .
Must Requirement :
Supply : 3.3V, Package thickness : 1.3mm under..
I recommended THS4304DGK but it's slew rate(830V/us) is lower than OPA693(2500V/us) so I think it will not good for 130M CLK buffer.
Would you recommend proper part for this requirement ?
Thanks,
JH Seo.