Part Number: INA210
Other Parts Discussed in Thread: TMS320F28027, , AMC1200, DRV421, INA180
Hello
I would like to measure the inductor current in an interleaved Boost converter (Input voltage: 10-60V; Output voltage max 120V, inductor current: 0-10A)
The current measurement is fed into a µC (TMS320F28027) for the PI current control loop.
For the moment I am using LEM current sensors as they provide galvanic insulation between the power and the signal stage. But they are rather bulky and take up a lot of space on my board.
I am thinking of measuring the current via a resistor in combination with the INA210 as it seems to me as a simple and robust solution with the lowest component count and small footprint.
I am however a little bit afraid about the fact that there is no isolation provided between the power and the signal part in this case.
s there anyone who would give me some advice in using this component for power electronics applications? Are there a lot of problems to expect? Do I need to take special measures to protect the µC...
I know that you also provide ICs like the AMC1200 (fully differential isolation amplifier) but this component requires a separate power supply on it's primary side. Since I have four of these current measurements, I prefer not to have that much separate power supplies as I suppose that the reliability of my board will strongly decrease.
Any help or comments are strongly appreciated since I have only little experience in this topic.
Kind regards
Simon