Tool/software: WEBENCH® Design Tools
Dear TI:
I want to achieve a Single-ended to differential circuit, the amplitude of the input signal is about -40dB, the bandwidth is about250MHz, so I choose THS4541 as the fully differential amplifier. the schematic diagram and PCB layout are as flow:
the power-supply is 3.3V, the Vcom is 1.65V by setting the resistance R7 and R9.
Then I test the circuit. the signal generator sent 0dB sine wave. one of the output pin is connected with spectrum analyzer. when the power is off, the amplitude of the peak shown on the spectrum analyzer is -40dB, the frequency is same with the signal sent by the signal generator. when the power is on. the amplitude of the peak decay a lot, about -70dB.
so,what happened about the circuit?
Is there some wrong in the parameter setting?
please help me