Part Number: PGA870
What is the valid range of DC offset which can be applied to the inverting input with gain at 0dB, and 20 dB ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PGA870
What is the valid range of DC offset which can be applied to the inverting input with gain at 0dB, and 20 dB ?
I wasn't referring to CM offset.
We want to purposely offset the output as seen by the ADC, and looking at how this can be best achieved.
Input is AC coupled to non-inverting input; and the inverting input is grounded by same capacitor value.
Can we simply apply an offset voltage (eg, DAC + buffer) to the inverting input?
We understand there will be a dependency on gain setting.
We are using the PGA870 to drive a fast ADC and also amplify a 1Vp-p signal of BW 220MHz which is AC coupled to the non-inverting input.
Inverting input is grounded via the same capacitor value, therefore at AC ground potential.
Is it possible to apply a DC potential to the inverting input via some form of DC coupling network to achieve a differential offset function at the differential output without affecting the common mode voltage?