Other Parts Discussed in Thread: TLV2463, OPA2373, TLV2373
Hi all,
I am using TLV2463, OPA2373 as a two-stage amplifier,single supply at 3.7V, non-inverting configuration, each theoritical gain = 150. signal frequency is 40kHz (ultrasonic receiver circuitry).
Shutdown pins are directly connected to VDD.
Output of the 2nd stage is connected to a diode-RC simple peak holder circuit.
i have some questions:
1. when it is measured, why the gain (Vo/Vi) is lower than 150.. it is around 40.
2. stage two (2nd op amp in the IC) always get damaged eventually. no idea why.
The output of the 2nd op amp is either stuck high or smthing else (will post a picture)
what could b the problem?