Part Number: LMC6081
Hi,
Is the NC pin a pin to which nothing can be connected?(Pin1/Pin5/Pin8)
Is the NC pin connected internally?
I want to connect as follows.
●Connection
V+ = +2.5V
V- = -2.5V
NC(pin1)= 0V
Non-inverting input(pin3)= 0V
Is there any problem?
Best regards,
Seishin