This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2902: LM2902 single supply characteristic question

Part Number: LM2902


My customer is trying to use the LM2902 in a single supply configuration (+3.3V) to amplify a small AC signal.  This signal swings around GND, but I only care about the positive signal being amplified.  There is a possibility that this input signal can swing to -1.0V peak in some conditions, but I can easily limit the current.

1)      How much current can the input’s reverse protection diode take?

2)      I can also add a clamping diode on the input to limit this to -0.25V peak.  I’m guessing if I do this, I don’t risk any damage to the part?

3)      Typical operation shouldn’t exceed -60mV peak on the input (with very low current).  I’m assuming this is fine for normal operation.

  • Steve,

    1) Input could survive over 50mA, however, don't do that. 10mA is a legacy standard rule. I personally recommend 1mA maximum.
    2) Limiting to -0.25V is best because any input current (via internal parasitic diode) could cause output to invert (Phase reversal).
    3) Yes, that is fine.

    At -40C, keep in mind that maximum output voltage (VOH) will be just over 1.3V (VCC -2V)