Part Number: DRV425
Hi Javier
Could I request the FEMM models along with any supplementary information for TIDUAZ4 reference design please? Both the standard +/- 100A as well as the modified version boosting the current rating.
I'm especially interested in knowing how low the magnetic fields are for very low currents and any thoughts on how to improve sensitivity at this very low end whilst still maintaining good accuracy at the top end. I'm assuming the wider the busbar the better... perhaps using a 1.0mm PCB rather than a standard 1.6mm might help (there is reference to "mounting, back to back, as close as possible" but I don't know if 0.6mm is going to matter).
Whilst I've never used the FEMM tool I'm hoping that with both the stock & modified model files (and any matching supplementary info) I can work out the best shape/size of busbar to suit the current range and modify accordingly. I don't know if the FEMM models you have to hand show a variety of busbar sizes and it's possible to switch between them to see the performance differences?
Any recommendations for the ADC (24bit delta sigma perhaps, but any other characteristics that would be beneficial?) that would well match this reference design?
Many thanks.
Jim.