Part Number: LMC6482
Other Parts Discussed in Thread: TINA-TI
Hi TI contributors,
I am faced with an unstability problem with the LMC6482 OpAmp used in comparator mode (because the function need in first a unity gain follower).
The function have to discharge a capacitor with pull-up resistor for OR-ed purpose (signal name : OU_STOP). When the input signal grows up above the threshold, it seem that the OpAmp output can not discharge the output capacitor (C52) and lead to the output voltage unstability :
MY OBSERVATIONS :
- I used previously the same design without problems.
- The TINA simulation did not give any clue of that behaviour, in TRANS, DC Gain with temperature full range.
- With the design values, the simulation shows an output current peak of #13 mA.
- If C52 is divide by ten (10nF), the output mean voltage is lower, but can not be drive low enough (still not stable).
MY QUESTION ABOUT LMC6482 :
- Is the LMC6482 has a overcurrent protection which can lead to this behaviour (not documented in datasheet) ?
- Is overtemperature protection of the LMC6482 is very sensitive to output current ?
- Does a output serie resistor addition in order to limit output current is mandatory ?
Thank you in advance for your answers !