Part Number: TLV3202
Other Parts Discussed in Thread: TLV3502
Support Path: /Product/Help with Device Selection/Amplifier/filter solution/
Good morning,
I'm designing an application based on a FPGA.
The chip needs fast transition at its inputs pins (rise and fall times < 10ns) to avoid totem pole current (which can lead to degradation of MTBF)
I'm thinking about using the TLV3202 to condition the input signals.
So my question is:
• are you able to specify the maximum 10%-90% rise time and fall time?
Indeed in the datasheet, only the typical values are given (respectively 4.8ns and 5.2ns)
If needed, you can consider the parasitic capacitance at the comparator output to be 50pF.
Thank you.
Best regards,
Gauthier Lemey