Part Number: OPA549
Other Parts Discussed in Thread: OPA564
Hi,
I want to build a current source (1A max), frequency: 50kHz to 100kHz, the load is a coil (350uH). I am working with the amplifier OPA549, but there is a temperature problem, I don't know why. I want to know if the OPA549 is the best option for this application or if there is another solution.
Regards,
Pablo