Other Parts Discussed in Thread: ACF2101, , IVC102
I need to evaluate an ACF2101 switched integrator. As it's surface mount I'd like to get an evaluation board.
The ACF2101 documentation says it works with the OPAMPEVM-SOIC opamp board, but it has 24 pins
and the board is speced to work with 8 14 and 16 pin chips.......so how do I use it with the ACF2101
or is the TI information wrong?
Also the original Burr Brown data sheet mentions a fully featured demo board DEM-ACF2101BP-C and it would
be great to get hold of one of those....is it still available?