Part Number: LM293
Hi all,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Toshi-san,
The LM293 is an open-collector comparator. Refering to LM293 datasheet Fig. 6, and connecting it as shown in your diagram shows that the output stage NPN open-collector is connected back to the base of the input PNP transistor. This would be an unusual circuit connection for a comparator. The actual output state of the comparator might be somewhat unpredictable because it would be dependent on the particular comparator's voltage offset, bias current and likely any noise introduced into the circuit.
If the LM293 common-mode input voltage (Vicr) weren't limited to Vcc - 1.5 V, a predictable output state could be achieved by simply connecting the one input to ground and the other to V+. However, because of that Vicr limitation the minimum component solution would be simply to ground both inputs and let the output pin float open. In that case, the output state will be determined by the voltage offset of the comparator. Since the output pin is open the output will simply be off if the offset is in one direction, or simply won't draw any collector current if the offset is in the other direction. If you don't like the idea of letting the output pin float, a very high resistance resistor such as 1 Megohm, could be added from the output to V+. The output will either be set high, or low, depending on the comparator's offset.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
I am using LM293 as a voltage windows comparator. To make input voltage stable, is it okay to add a smaller capacitor on each input of comparator?
Thanks,
Tony