Part Number: OPA548
Hi. I have a question related to the SHUTDOWN mode of OPA548. I have been testing the circuit shown in the image below. The OP amp is configured as a follower, with an input voltage of 3.5V. The OP amp is in shutdown mode, as the pin E/S is LOW. With this configuration, is it possible to apply 4V2 at the point labeled with "4.2 V"? Could this configuration damage the OP amp? This situation could be present in the real design, so I need to be sure that all is ok. Thank you in advance for your help!!!