Part Number: OPA875
I am looking for some help finding a replacement for the AD 8015 (See attached spec sheet. The AD8015 is a very old die and the company I work for would like to move away from it before it goes into end of life. The ideal replacement would have as few connections as possible and must be in Die form. We are using the amp for reading a photo diode and the in and out must go down to DC. Our bandwidth requirements are not very high << 100MHz. We would also like to reduce the signal noise as well.