This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV324: issue with lmv324 buffer output limits to 2.7v

Part Number: LMV324


HI ,

iam using LMV324ID AS a buffer ,

VCC 3.3V, but out of the buffer is latching to 2.71 to max of 2.74.  even my buffer input crossing 3V.. why ? any limitation in the part ? i am expecting buffer out put should follow the input .

Please help me .