Part Number: INA196
Other Parts Discussed in Thread: INA195
Hi there !
In the datasheet, under Absolute Maximum Ratings the input voltage is given with -+/ 18Volts. How can the common mode voltage then be -16/ + 80 volts ?
Thank You !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joseph,
Thank you for using the E2E Forums.
Our manufacturing process allows us to have common mode voltages that exceed the device supply. This is a very common requirement, where the parts are fed at a lower voltage (as low as 3V3 to interface with an mcu or other logic) but are required to measure voltages on a higher voltage bus.
So to clarify, these values are correct.
Hi Joseph.
Just an update to my previous reply, as I might have misunderstood your original question:
I have verified and for this particular device (INA195), there is indeed a error or the datasheet, since the AMR for inputs are stated as to -18 to 18V.
Table 7.1 should look as below:
Thank you for noting this. I will ask our team to correct the datasheet.