Part Number: XTR117
Other Parts Discussed in Thread: XTR117, XTR111
Support Path: /Reference designs/Technical support help for a specific technical issue with a reference design/
I am using the XTR117 current loop transmitter in my design. I have powered the input circuit from the Vreg pin of the IC with Iret as the return path, as instructed in the datasheet. But I need to drive another XTR117 from this same input circuit (being powered by the first XTR as previously described). If I connect the Iret pins of the two XTR117 ICs together and drive both the ICs from the same input circuit, will it work fine?