hello!
I do not have a lot of basic electronics background but I need a simple photodiode amplifier circuit for my project. The optical beam received has intensity of a few microwatts and the photodiode amplifier circuit is needed to convert the optical signal into a voltage one. I am using a Hammamatsu diode, chose OPA129 for this and designed the whole circuit exactly with same component values as shown in figure 7 of OPA129 datasheet (http://focus.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=sbos026a&fileType=pdf ). It is supposed to be a simple circuit where I come in with an optical signal of some microwatts and get it in voltage after passing through the amplifer but what I get at the output is fixed -15V which is the supply voltage at pin 5. Like I said I do not have a lot of basic electronics background and after some reading on the internet i think it maybe as I designed my PCB exactly as shown in fig.7 of above datasheet and in that figure they do not have any input resistance at input 2 of amplifier. Is this the reason why the photodiode amplifier is not working as it should? Additionally it was hard for me to conceive how to design the guard ring so I just grounded inputs 1,3,4 and 8 on the board which I now think is wrong. I can not progress ahead until this problem is solved so please any hep will be sincerely appreciated.