Part Number: LMH6554
Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
Hello,
I have a circuit with LMH6554 which used like a single to diff converter at the input of the ADC which has 1.25V common voltage requirements. So, I prepare schematic based on SNOA565A (www.ti.com/.../snoa565a.pdf). But in my case input signal has Vcm = 2V and it should be DC-coupled.
It is TINA schematic - LMH6554_single_to_diff.TSC- here I use not equal Rpu resistors in order to achieve output common voltage 1.25V for both outputs. Is it correct or not? And is there another option to achieve Vcmi = Vcmo?
Thank you!
Tsa