Other Parts Discussed in Thread: OPA656
I am using OPA656/657 in liquid nitrogen temperature. And wanting to measure the input current noise of OPA656/657. From their datasheet, their input current noises are as low as 1.3 fA/sqrt(Hz). It means that I have to put a resistor as large as 10G in its input stage to make inRs override sqrt(4kTRs).
From their datasheet, I find the common mode input capacitance of OPA656/657 is 2.8pF/4.5pF. The impedances of these capacitance is far small than 10G above a frequency like 1kHz. I guess thess capacitance will bypass the input current noise of OPA656/657 and make the measurement fails.
I wonder if this method can work. But if not, can anyone tell me how manufacturer like TI measure such low input current noise?