Part Number: LM7322
Hi,
May I understand if LM7322 is able to take 0 to 30V for both supply voltages and signal?
Is the positive max clamp at +15V?
Thanks,
Christina
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM7322
Hi,
May I understand if LM7322 is able to take 0 to 30V for both supply voltages and signal?
Is the positive max clamp at +15V?
Thanks,
Christina
The absolute maximum ratings for the LM7322 are shown in Section 7.1 of the product datasheet. I've copied the table below for reference. The absolute maximum supply voltage is +35V, so supplies voltages less than or equal to the absolute max rating will not cause damage to the device.
The recommended supply voltage range is +2.5V to +32V which is the range where the product specifications are valid over.
The absolute maximum ratings for the input/output are relative to the supply voltage and can be +/-0.8V outside the supply voltages without causing damage.
This device also features differential input clamps which require that the absolute maximum differential voltage between IN+ and IN- to be at most +/-10V. This is typically not an issue unless trying to operate the device as a comparator or as a buffer with very fast changes to the input voltage.