Part Number: THS4521
Hello,
We use a THS4521in front of an ADC input on this configuration :
Signle ended to differential
Single supply +5V
VOCM is left floating
Gain = 5.36 = R2/R1, with R1 =261 Ohms and R2 = 1400 Ohms
It woks well and I supply is about 2 mA (load = 2.2 KOhms, with sinus CW 10 KHz , level=2.4 Vp on output for instance) when the amplifier is in linear mode (no saturation).
But when its goes to saturation mode (Vin * Gaion > 2.45 Vp) the power consumption of the amplifier THS4521 rises to 7 mA instead of 2 mA.
Could you explain this over-consumption under saturation ?
A standard AOP does not react like that.
best regards
thanks
A.C.