Hi team,
The customer is using OPA548. Can the exposed pad for OPA548 be connected to GND?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
The customer is using OPA548. Can the exposed pad for OPA548 be connected to GND?
Hi Mickey,
The metal tab of the OPA548 TO-220 and DDPAK packages is internally connected to V-. Therefore, the tab must be connected to the same potential as V-, or it must be insulated from any other potential to prevent an electrical connection, i.e. use a mica insulator, or non-conductive thermal pad, and insulating hardware. If the OPA548 application circuit uses a single positive supply and GND, and V- is connected GND, then that satisfies the electrical connection requirments. If a dual supply V+ and V- is being used, then the tab must be connected to V-, or insulated from GND.
For more information see section 11.1.2, Amplifier Mounting, in the OPA548 datasheet.
Regards, Thomas
Precision Amplifiers Applications Engineering