Part Number: INA826
Hi all,
I'm considering a INA826 for a high output impedance current source. I don't care much about the exact current but about the stability.
The current must not change for different loads. (100-150ohms @ 1mA & 1-1500ohms @ 100µA)
This has to be ensured for several years (e.g. ~10000h)
Therefore, I have to take the long term stabilty of the amplifiers gain into account.(rather than the offset voltage drift)
As you can see in the picture, (difference amplifier of the instrumentation amp) the ratios R6/R7 or R1/R2 should remain exactly the same.
Could anyone give me an approximate value of how much gain-drift we have to expect?
TemperatureRange: 0-70°C
Load: no Load (input of voltage buffer)
Best Regards and thanks in advance,
Achim Schäfer