Part Number: OPA140
Other Parts Discussed in Thread: OPA827
Tool/software: Code Composer Studio
Dear Support,
I am considering OPA140 as a Unity gain buffer to interface a 50 Ohm spectrum analyzer with a high-Z source.
Frequency range of interest is 1 Hz-1000Hz, so flicker noise is a major concern. Being the source in the high-Z
range (>10k, up to 1M), current noise has to be very low. The FET input stage makes the OPA140 a natural choice,
in my opinion. Power come from 2x 9V batteries, for best noise performance.
Can you confirm my analysis ? Please suggest any other solution, if more appropriate.
I need to drive a 50 Ohm load (the instrument) with minimun distortion and noise as low as possible
(we need to measure noise Power Spectral Densities of other devices).
Could be better to place in parallel 2 or more OPA140 ? If so, can you give me any advice ?
Thank you in advance for your help.
Regards,
Alberto