Hi,
A unity gain OPA350 is driving a 10 ft RG-58 cable terminated in an AC-Coupled 50 Ohm input spectrum analyzer.
A circuit schematic is pasted below. The OPA350 is powered by a +5V single supply. ALA_MID is at 2.5V.
The two inputs that are summed are outputs of a high-gain 200 kHz and 300 kHz band-pass filter.
In addition to the desired signals, the spectrum analyzer is showing an oscillation at 109-112 kHz of significant amplitude.
When the output is connected to a nearby scope (2 ft of coax), there is no oscillation.
Another clue is that when the inputs to the summing amp are reduced, there is no oscillation.
Placing 100 ohms in series with the OPA350 output eliminated to oscillation, but 50 ohms had no effect.
Any insights would be appreciated.
Thanks