Part Number: OPA211
Dear Team,
I ordered OPA211AIDR in this part marking is OPA211A but I receiving OPA211K.
What is the difference between marking the part of OPA211A and OPA211K.
Best regards,
Muthu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA211
Dear Team,
I ordered OPA211AIDR in this part marking is OPA211A but I receiving OPA211K.
What is the difference between marking the part of OPA211A and OPA211K.
Best regards,
Muthu
Hi Muthu,
The OPA211AIDR is the high-grade device. When you view the device with pin 1 in the lower left corner you should see an "A" near the upper left corner indicating an A-grade device. The "K" after the "211" has a meaning that pertains to TI's internal manufacturing. A standard grade OPA211IDR may have this same "K" code marked on it.
If the device is marked as I have described you have received the correct device.
Regards, Thomas
Precision Amplifiers Applications Engineering