Part Number: AMC1301
Hi all
Would you mind if we ask AMC1301?
In case of Isolated Voltage Sensing, we can understand that a series resistor is recommended to be used at the negative input (VINN) of the AMC1301 device with a value equal to the shunt resistor R3 (that is, R3' = R3 in Figure 52) to eliminate the effect of the bias current.
So, in case of Isolated Current Sensing, should sense resistance R3 value be equal to R3' value?
Or, the shunt resistance R3 is very small vaule, so it is not necessary to consider the bias current, right?
Kind regards
Hirotaka Matsumoto