This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1815: Variable Reluctance Sensor for measuring Torque

Part Number: LM1815

Hi,

I would like to know if the LM1815 is suitable for my application. I want to interface it

to the output of a variable reluctance sensor for use in measuring torque.

The output of the sensor  is non-sinusoidal  with an output voltage which can vary between 0.75V to 12V peak to peak at a frequency of

approximately 40Khz. The spec for the sensor states that the load impedance should be at least  200k Ohm.

Any assistance in determining if the LM1815 will do the job for me would be much appreciated.

Thanks,

Eliot