Part Number: LM741
Test conditions in data-sheet suggests that TA =25°C,VS =±20V for input resistance to be ~2 MOhms. I need schematic of test-bench so that I can validate this on bench.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jay,
Do you have access to a meter that can read in the nano-amp (1nA resolution) range?
Both inputs are NPN bases which act like current sources. As input difference voltage changes the balance of these current source shift to one side or other based on polarity of input difference.
Is there a reason to test this parameter?