Part Number: INA240-Q1
Hello,
For the INA240-Q1, if the differential voltage on the pins is applied at max rating i.e. 80 V, is this operation mode time dependent ?
Also, in case the difference between the inputs is high (max rating), what is the protection circuit used to avoid failing of the device?
On what parameters is the recovery time of the device calculated?
Thanks.
Nikhil