Part Number: PGA202
Hi,
I supply PGA202 from +/-18V and in this case is it possible to apply to the non-inverting input +15V if the inverting input is grounded.?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PGA202
Hi,
I supply PGA202 from +/-18V and in this case is it possible to apply to the non-inverting input +15V if the inverting input is grounded.?
Hello Alex,
Yes it is possible. According to the input range vs power supply graph, using a supply of +/-18V allows for an input of up to 16V. Keep in mind, however, that the output swing has a limit at around 12V and since the minimum gain for this part is at 1, the output will saturate at this limit.
Regards,
Hasan