Part Number: ISO124
Hello,
I am calculating the iso amp output error range. Can you advise if the following calculation is correct?
output voltage Vo = (Gain +/- Gain_error + Gain_error_temp)*(Vin +/- Vos)*(1+/- NL). Vos is input offset voltage. NL is nonlinearity.
If the input is 2Vdc, then the max possible output at 85C is ( using ISO124 spec): Vo_max = (1+0.5%+10E-6*(85-25))*(2+0.05)*(1+0.01%) = 2.062 V.
Let's don't consider the Vos temperature variation for now.
Thanks.
Zhenyu