Other Parts Discussed in Thread: OPA188, THS3125, , OPA659, OPA656
Hi,
I would like to understand a little better the mechanism that the OP380 uses in order to have a low output DC offset while being a current feedback op-amp. In the datasheet it mentions it has another internal op-amp which is auto zeroing connected into the non inverting pin like this:
Could the same strategy be used with any current feedback op-amp? For example if I wanted to create a composite op-amp with the THS3125 and OPA188.
Thank you!