Part Number: TLV4112
This could be me struggling with reading the datasheets, but I couldn't find the ratings for this amplifier.
I want to power this amplifier with +/-5V power supply. In page 3 (absolute maximum ratings), the differential input voltage is +/-VDD, and VDD is 7V. However, in the layout in page 2, it shows VDD and ground.
Does this mean I can use +/-5V. Or can do I have to use lower voltages i.e. +/-3V?
Also, does the power supply have to have high current rating if I am using high output current. For example, If I am drawing 300mA out of the output, does the power supply have to match this (>300mA), or does it just satisfy the input current (700uA/channel typical)?
Thank you very much in advance,