Other Parts Discussed in Thread: LMC6482
I am trying to use LTV4112 as a dual op-amp circuit to interface with an electrochemical sensor.
The operation depends on having high output current (max 360mA) but low input bias current.
I measured the input bias current to be 1-1.7nA at 350mA output current. However, the data sheet shows input bias at 0.2pA (typical) to 25pA (max).
Is this typical for the this part number? Or is it an indication that I am using this incorrectly? Also, if you're aware of any other op amps that can be used as a substitute, please let me know.
Attached is the circuit under discussion. The "dummy cell" is a replacement for the electrochemical cell for testing purposes. I tried adding 260ohm resistor which limited the current from 1.7nA to 1nA.
Thank you very much in advance.