Other Parts Discussed in Thread: INA138, , TINA-TI
Hi all,
Since now we are developing a product which need to current sensing of the load (100mA to 7A full range) by 30V supply, then input to MCU A/D for current measurement, before I was use INA138 to achieve it, because change to battery supply, so now we need to takecare the current consumption by the INA138 also, I was find that the op amp TLV8802 current consumption is suitable for our usage, but I have some question:
1. Can I use TLV8802 instead of INA138?
2. Is it suitable usage for High side detection or low side only?
3. Any other IC suggestion use current sense with low current consumption?
Thanks all for help!