This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM293: Why does the datasheet give conflicting information on the comparison polarity???

Part Number: LM293


In the datasheet for the LM293 and other variants of this comparator, Section 7.3 states:

The output NPN will sink current when the positive input voltage is higher than the negative input voltage and the offset voltage.

In the same datasheet, section 8.2.2.1 states:

If IN- is higher than IN+ and the offset voltage, the output is low and the output transistor is sinking current

I find this odd.  And by 'odd', I mean really conflicting.

Please explain.

  • Hello John,

    Yes. We are aware of this. We have corrected it and the revised datasheet should be released soon.

    Below is the updated text:

    The following is a list of input voltage situation and their outcomes:

    1. When both IN- and IN+ are both within the common-mode range:

    (a) If IN- is higher than IN+ and the offset voltage, the output is low and the output transistor is sinking current.
    (b) If IN- is lower than IN+ and the offset voltage, the output is high impedance and the output transistor is not conducting.

    2. When IN- is higher than common-mode and IN+ is within common-mode, the output is low and the output transistor is sinking current.
    3. When IN+ is higher than common-mode and IN- is within common-mode, the output is high impedance and the output transistor is not conducting.
    4. When IN- and IN+ are both higher than common-mode, the output is low and the output transistor is sinking current.